emWin 5.20

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emWin 5.20

1,843件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Harvey_13 on Tue May 21 08:06:22 MST 2013

I uploaded the new version of emWin for NXP


When I tried to compile, I got some errors : <strong>GUI_pMem</strong> and GUI_MemSize not found !!!!


I compared with the former version and saw there are some differences on GUIConf.c


I added the line


<code>#define GUICONF_C</code>


at the beginning of this file and now it compiles correctly.


Is it normal ?


<span><span class="hps">Does</span> <span class="hps">anyone seen</span> <span class="hps">this problem?</span></span>


 


 


ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,799件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Harvey_13 on Wed May 22 04:35:16 MST 2013

Finally I download the file through another connection  : It compîles with no error.


<span><span class="hps">But</span> <span class="hps">this is not</span> <span class="hps">really</span> <span class="hps">the same environment</span>
<span class="hps">I use</span> <span class="hps">μEz</span> <span class="hps">as</span> <span class="hps">multitasking</span> <span class="hps">kernel and my </span><span class="hps">needs are not</span> <span class="hps">the same</span>

<span class="hps">As</span> <span class="hps">it worked</span> <span class="hps">with</span> <span class="hps">the previous version</span> <span class="hps">I</span> simply <span class="hps">recover the former files</span> :
<span class="hps">GUI_X_uEZ.c</span><span>,</span> <span class="hps">GUIConf.c</span> <span class="hps">and</span> <span class="hps">previous</span> <span class="hps">LCDConf.c</span> <span class="hps atn">(</span><span>referenced</span> <span class="hps">emWin</span> <span class="hps">v5.06</span><span>)</span>

<span class="hps">And it</span> <span class="hps">compiles</span> <span class="hps">correctly</span></span>


<span><span class="hps">Sorry </span></span><span class="short_text"><span class="hps">for the inconvenience.</span></span>


<span class="short_text"><span class="hps">Thanks
</span></span>

0 件の賞賛
返信

1,799件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Harvey_13 on Wed May 22 01:39:51 MST 2013

Hi,


In fact I could not succed<span><span></span> <span class="hps">to</span> <span class="hps">download this file</span>
<span class="hps">I have a</span> <span class="hps">systematic error</span> <span class="hps">at the end of</span> <span class="hps">loading</span></span>


 


Regards<span><span class="hps">
</span></span>

0 件の賞賛
返信

1,799件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue May 21 19:29:40 MST 2013

Hi Harvey_13,


Did you try BSP from 


<a href="http://www.lpcware.com/content/nxpfile/emwin-520-board-support-package-ea1788-board">http://www.lpcware.com/content/nxpfile/emwin-520-board-support-package-ea1788-board</a>


 


Thanks,


NXP Support

0 件の賞賛
返信