dual core DMA restriction?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dual core DMA restriction?

1,417件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jpplus on Sun Jan 11 22:04:19 MST 2015
Hi all,
I have an audio application running on LPC4337. The I2S and SGPIO will be configured to trigger DMA both on M0 and M4. As I need access DMA controller from two cores, my question are:
1) can chip  genereates DMA interrupt for DUAL core in same time?
2) can I init the DMA controller in one core and use that and generate interrupt in another core?
3) can IS2 is init in one core and generate DMA interrupt in another core?

I think DMA only need to be init in one core as there is only one DMA hardware, but can be directly operated from both core.
I am new to this chip, but hope to get some hints on this two core DMA stuff.
thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,327件の閲覧回数
nos1989
Contributor II

I'd like to bump this discussion up as I'm curious about the same thing.

0 件の賞賛
返信