download source file cr_startup_lpc176x.c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

download source file cr_startup_lpc176x.c

867 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by engineer1 on Mon Apr 07 03:58:55 MST 2014
hi
I Want porting emWin library for lpc1768
So i need source file cr_startup_lpc176x.c
help me for download cr_startup_lpc176x.c
thanks
标签 (1)
0 项奖励
回复
1 回复

832 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Apr 07 04:51:46 MST 2014
cr_startup_lpc176x.c is the entry point and startup file for LPCXpresso IDE only. When you use the LPCXpresso 'New Project" wizard, it is created automatically for you. If you are not using LPCXpresso IDE, you will need the startup file for the toolchain that you are using.
0 项奖励
回复