does emWin from NXP include GUIDRV_FlexColor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

does emWin from NXP include GUIDRV_FlexColor?

2,466件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ivan Sylvan on Fri Jun 15 00:08:34 MST 2012
Hello!
I'm trying to use emWin with LPC1768 and ILI9335 controller. And i've downloaded emWin from nxp.com. It contains GUI.lib but i don't know if this library file contains GUIDRV_FlexColor?
The second question is should i write my own GUI_PORT_API routines like pfWrite16_A0 and others? Where can i see the samples of this API routines?
Thanks in advance.
Ivan.
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,391件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ivan Sylvan on Thu Jul 19 22:59:18 MST 2012
Thanks a lot!
0 件の賞賛
返信

2,391件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ivan Sylvan on Thu Jul 19 22:58:45 MST 2012
Thank you so much, Wouter! :)
0 件の賞賛
返信

2,391件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wouter on Wed Jul 18 05:18:59 MST 2012
Hi Ivan,

Please have a look at the MCB1700 BSP:
http://www.lpcware.com/content/nxpfile/nxpemwin514mcb1700bsp

This uses the LPC1769 together with a FlexColor display.

Regards,
Wouter
0 件の賞賛
返信

2,391件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Jul 16 11:07:19 MST 2012
Hi Ivan,
Yes, the emWinlibrary supports GUIDRV_FlexColor. I suggest you to check GUIDRV_FlexColor.h in the BSP.
Ilitek ILI9335 is supported in emWin Library 5.16.

Please go through emWin user manual.
0 件の賞賛
返信