difference between FIODIR & IODIR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

difference between FIODIR & IODIR

4,569 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moslem1368 on Sun Dec 02 02:59:49 MST 2012
Hi
What is difference between FIODIR &  IODIR Reg. in lpc21xx in Aplication?
Labels (1)
0 Kudos
Reply
2 Replies

3,988 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Aug 15 15:50:45 MST 2013
Hi,

FIODIR refers to Fast Input/Output Direction control register and IODIR refers to Input/Output Direction control register. The purpose of FIO is basically application oriented. In case you have a external memory running at high frequencies and you want to communicate with it. Here, FIO's are better than IO's as they are faster.

Thanks,
SK
0 Kudos
Reply

3,988 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by omid.azadeh on Mon Apr 08 01:43:57 MST 2013

hi


FIODIR -> Fast Input/Output Direction


IODIR -> Normally Input/Output Direction

0 Kudos
Reply