deep sleep standard timer running

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

deep sleep standard timer running

跳至解决方案
2,638 次查看
simonwyss
Contributor III

Is it possible to let the standard timer (0/1/2) run in deep-sleep. I think in the user manual is written no:
pastedImage_1.png

For a wireless application I need to track time. If possible with a resolution of 32us. Therefore I used the timer 0 with a external 32kHz crystal as RTC clock. The RTC clock is used in sleep-mode for the timer 0. But in deep-sleep this didn't work.

Do I have to use the RTC-Timer (Alarm), to keep track of time? 
I would like to have a 32kHz Timer in low-power mode meanwhile the RTC seems to be max 1kHz (wakeup-timer). 

Is there a solution for my question?

标签 (1)
0 项奖励
回复
1 解答
2,474 次查看
simonwyss
Contributor III

It seems not possible to let digital peripherie running in the power-down mode.

I solve this with the 32bit rtc timer. Keep in mind, that the RTC has 2 internal timers:
1x 16bit one-shot timer, counting down to zero, 1kHz input
1x 32bit rtc, counting up endless, 1Hz input

I set a rtc alarm, after wakeup I update my 32kHz fast internal timer with 32000*rtc_time_passed.

pastedImage_1.png

在原帖中查看解决方案

2 回复数
2,474 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Simon Wyss,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
If you have any further questions about it, please feel free to contact with me.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,475 次查看
simonwyss
Contributor III

It seems not possible to let digital peripherie running in the power-down mode.

I solve this with the 32bit rtc timer. Keep in mind, that the RTC has 2 internal timers:
1x 16bit one-shot timer, counting down to zero, 1kHz input
1x 32bit rtc, counting up endless, 1Hz input

I set a rtc alarm, after wakeup I update my 32kHz fast internal timer with 32000*rtc_time_passed.

pastedImage_1.png