ctimer match value and prescale value for 25 clock pulse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ctimer match value and prescale value for 25 clock pulse

1,338 Views
sachinn434
Contributor I

 


hi  everyone i am using lpc54so18 evk board 

i need generate 25 clock pulse for encoder input so i am developing  SSI protocol with gpio toggle so i am facing issue with ctimer i need to how to set match value and prescale for 250kz frequency and match value for 25 times interrupt generation so please help any one 

thanks 

PRINTF("SSI INTERFACE USING GPIO\r\n");
srcClock_Hz = CTIMER_CLK_FREQ;
PRINTF("CTIMER_CLK_FREQ %d\r\n",CTIMER_CLK_FREQ);
CTIMER_GetDefaultConfig(&config);
config.prescale = CTIMER_CLK_FREQ /1000 - 1 ;// 1ms tick

// timerClock = srcClock_Hz / (config.prescale+1);

//PRINTF("timerclock %d\r\n",timerClock);

CTIMER_Init(CTIMER, &config);
matchConfig.enableCounterReset = true;
matchConfig.enableCounterStop = false;
matchConfig.matchValue = 25;//timerClock/480;//timerClock/2; //timerClock/0.024;//CTIMER_CLK_FREQ;//CTIMER_CLK_FREQ/4000000;
PRINTF("matchValue %d\r\n",matchConfig.matchValue);
matchConfig.outControl = kCTIMER_Output_Toggle;
matchConfig.outPinInitState = true;
matchConfig.enableInterrupt = true;

0 Kudos
Reply
1 Reply

1,311 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I suggest reviewing the SDK there has an example with the CTimer and I think that could be helpful the example has a LED toggle. I recommend not using a printf if you want to use a little time base.

Example documentation.
The CTimer Example project is to demonstrate usage of the KSDK ctimer driver.
In this example, the match feature of the CTimer is used to toggle the output level.

Best regards,
Pavel

0 Kudos
Reply