crt_directory2.xme

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

crt_directory2.xme

1,946 次查看
richard_brisk
Contributor I

cannot find crt_directory2.xme in the usual places.  Cannot continue

标签 (1)
0 项奖励
回复
1 回复

1,649 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Richard,

 

Just to be sure, did you look in the following path?

 

C:\nxp\MCUXpressoIDE_10.3.0_2200\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_10.3.0.201811280239\binaries

 

Are you working on MCUXpresso? Could you try reinstalling MCUXpresso and check if this solves the problem?

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复