cortex debug connector...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cortex debug connector...

2,563 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by edsut on Wed Jun 26 15:25:05 MST 2013

I'm working with an LPC4330-Xplorer Board (<a href="http://www.element14.com/community/roadTests/1117">http://www.element14.com/community/roadTests/1117</a>) and I need to get a ribbon cable that has the 10-pin .05" header (for the xplorer board) on one end and a 10-pin .1" header on the other end.  Anybody know where I can get that?

Labels (1)
0 Kudos
Reply
5 Replies

2,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by edsut on Fri Jun 28 03:17:01 MST 2013

The SimpleCortex board definitely uses .1" spaced header (I have one); so apparently, this is a non-standard connector style for this purpose.  Actually, though, just looking again at the picture on <a href="http://www.brc-electronics.nl/">http://www.brc-electronics.nl/</a>, it DOES show what appears to be a .05" spacing header!  That's different than my board.  Hmmm... didn't even notice that.  Bottom line is I have this board, so I guess I'll just have to build up a cable myself.


Thanks

0 Kudos
Reply

2,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Thu Jun 27 09:32:14 MST 2013
You should check, but to me it looks like both boards have the small 0.05"pitch connectors.
0 Kudos
Reply

2,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by edsut on Thu Jun 27 04:06:52 MST 2013

I'm playing with a SimleCortex board (<a href="http://www.brc-electronics.nl/">http://www.brc-electronics.nl/</a>).  As appears to be the case with many of these eval boards, the debugger is built right onto the board, but is also configured so that the debugger can be used to connect to other boards (a switch on the simplecortex allows it to be disconnected from the onboard LPC1769).  Anyway, on that board there is a 10-pin .1" spacing header that I was assuming would be the "other" end of the cable I was hoping to buy.

0 Kudos
Reply

2,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by edsut on Thu Jun 27 04:01:34 MST 2013

I was hoping to play with the debugger that is built into the "SimpleCortex" board (<a href="http://www.brc-electronics.nl/">http://www.brc-electronics.nl/</a>).  It has a 10-pin .1" spacing header that I've been assuming is the "other" end of the cable that I need.

0 Kudos
Reply

2,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Thu Jun 27 00:43:12 MST 2013

A 10-pin .1" header is unusual, do you mean 20-pin?


What debugger do you use, maybe it supports the fine pitch cable directly (e.g. ULINK2 does)?


The connector is a Samtec FFSD, you can get it at Element 14 among others.


See also http://infocenter.arm.com/help/topic/com.arm.doc.faqs/attached/13634/cortex_debug_connectors.pdf

0 Kudos
Reply