clock cycle activity for LPC1114

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

clock cycle activity for LPC1114

3,321件の閲覧回数
heaton_1991
Contributor I

I am now working with the LPC1114 which utilizes the ARM CORTEX M0 architecture. I have one question about the instruction set summary of the ARMv6M Thumb instruction set. I want to know what the processor does during each single clock cycle for each instruction. For example, if I have the following code where I want to write something to the GPIO0DATA register to change the level of the IO output (Actually toggle PIO0_3) 
loop 
LDR R0, =(0x50003FFC); GPIO0DATA Base + 0x3FFC, address 0x5000 3FFC 
LDR R1, [R0]; 
MOVS R2, #(1<<3); 
; Store the value of R1 into GPIO0DATA 
EORS R1, R1, R2; 
STR R1, [R0]; 
B loop 
Question 1: 
Let's say the first clock cycle is when the chip fetches the LDR R0, =(0x50003FFC) instruction.  what the chip does in the following clock cycles? Also if there is any reference that could explain it, that will be really helpful. 

Question 2: 
I find that the time between PIO0_3 is toggled every 15 cycles. However, based on the instruction set summary, it should be 11 cycles (LDR/STR takes two cycles and MOVS, EORS takes 1 cycle, B takes 3 cycles), anyone knows why? If there is a timing diagram to explain it, that would be great! 

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,114件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Liao,

I suppose that you can modify your code as following to save instruction cycle time.

LDR R0, =(0x50003FFC); GPIO0DATA Base + 0x3FFC, address 0x5000 3FFC
loop:LDR R1, [R0]; 
MOVS R2, #(1<<3); 
; Store the value of R1 into GPIO0DATA 
EORS R1, R1, R2; 
STR R1, [R0]; 
B loop 

Because the R0 is not changed in the loop, so you can move loop label in the next line to save cycle time.

Question 1: 
Let's say the first clock cycle is when the chip fetches the LDR R0, =(0x50003FFC) instruction.  what the chip does in the following clock cycles? Also if there is any reference that could explain it, that will be really helpful. 

 >>>>>>The line LDR R0, =(0x50003FFC)  is a macro, it is replaced with two movs instruction. As you know that the Cortex-M0 core instruction is word(32 bits) or half word(16 bits),because the operand 0x50003FFC is 32 bits so it is replaced by two moves instructions.

Question 2: 
I find that the time between PIO0_3 is toggled every 15 cycles. However, based on the instruction set summary, it should be 11 cycles (LDR/STR takes two cycles and MOVS, EORS takes 1 cycle, B takes 3 cycles), anyone knows why? If there is a timing diagram to explain it, that would be great!

>>>>>I do not know where you get the cycle time of each instruction, anyway, because of pipeline, maybe the jump instruction B occupies multiple cycles. The Cortex-M0 is ARM IP, I suggest you ask ARM company directly, we have not detailed doc about the core.

Hope it can help you

BR

Xiangjun Rong

0 件の賞賛
返信

3,114件の閲覧回数
heaton_1991
Contributor I

Hi, Rong,

You mentioned that "The line LDR R0, =(0x50003FFC) is a macro, it is

replaced with two movs instruction", Could you please explain what the two

movs instructions are?

Thanks,

Haohao.

xiangjun.rong <[email protected]> 于2018年11月28日周三 上午1:03写道:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: clock cycle activity for LPC1114

reply from xiangjun.rong

<https://community.nxp.com/people/xiangjun.rong?et=watches.email.thread>

in LPC Microcontrollers - View the full discussion

<https://community.nxp.com/message/1085134?commentID=1085134&et=watches.email.thread#comment-1085134>

0 件の賞賛
返信

3,114件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Liao,

Anyway, the LDR Rd=constant is a pseudo-instruction, maybe different compiler deal with in different way.

This is the part I find in DUI0801E_armasm_user_guide.pdf

Hope it can help you

BR

XiangJun Rong

6.7 Load immediate values using LDR Rd, =const
The LDR Rd,=const pseudo-instruction generates the most efficient single instruction to load any 32-bit
number.
You can use this pseudo-instruction to generate constants that are out of range of the MOV and MVN
instructions.
The LDR pseudo-instruction generates the most efficient single instruction for the specified immediate
value:
• If the immediate value can be constructed with a single MOV or MVN instruction, the assembler
generates the appropriate instruction.
• If the immediate value cannot be constructed with a single MOV or MVN instruction, the assembler:
— Places the value in a literal pool (a portion of memory embedded in the code to hold constant
values).
— Generates an LDR instruction with a PC-relative address that reads the constant from the literal
pool.
For example:
LDR rn, [pc, #offset to literal pool]
; load register n with one word
; from the address [pc + offset]
You must ensure that there is a literal pool within range of the LDR instruction generated by the
assembler.

0 件の賞賛
返信

3,114件の閲覧回数
heaton_1991
Contributor I

Hi, Rong,

Many thanks for your help! I really appreciate it!

xiangjun.rong <[email protected]> 于2018年11月29日周四 上午2:35写道:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: clock cycle activity for LPC1114

reply from xiangjun.rong

<https://community.nxp.com/people/xiangjun.rong?et=watches.email.thread>

in LPC Microcontrollers - View the full discussion

<https://community.nxp.com/message/1085904?commentID=1085904&et=watches.email.thread#comment-1085904>

0 件の賞賛
返信

3,114件の閲覧回数
converse
Senior Contributor V

One reason for code executing more slowly than you expect is that the code is executing out of Flash, which can introduce wait-states.

0 件の賞賛
返信