changing the AHB Matrix priorities

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

changing the AHB Matrix priorities

2,178 Views
ankish_kacktwan
Contributor I

How can we change the AHB Matrix priorities in lpc1779 device?

Labels (1)
0 Kudos
Reply
3 Replies

2,093 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

LPC177x has Matrix Arbitration register
The Matrix Arbitration register provides the ability to change the default AHB Matrix arbitration priorities.

Please see MATRIXARB in UM.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,093 Views
ankish_kacktwan
Contributor I

can it be changed for LPC1778 device as well 

because i can not see any MATRIXARB register in LPC177x_8x.h

0 Kudos
Reply

2,093 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

According to UM, Matrix Arbitration register physically exists in LPC177x/8x. 

I check one of lpcopen, lpcopen_2_10_lpcxpresso_ea_devkit_1788, MATRIXARB is defined in sysctl_17xx_40xx.h.

if your project don't have it, you can define it as below:

#define MATRIX_ARB  (*(volatile U32*)(0x400FC188))
  MATRIX_ARB = 0            // Set AHB Matrix priorities [0..3] with 3 being highest priority
               | (1 <<  0)  // PRI_ICODE : I-Code bus priority. Should be lower than PRI_DCODE for proper operation.
               | (3 <<  2)  // PRI_DCODE : D-Code bus priority.
               | (0 <<  4)  // PRI_SYS   : System bus priority.
               | (0 <<  6)  // PRI_GPDMA : General Purpose DMA controller priority.
               | (0 <<  8)  // PRI_ETH   : Ethernet: DMA priority.
               | (3 << 10)  // PRI_LCD   : LCD DMA priority.
               | (0 << 12)  // PRI_USB   : USB DMA priority.
              ; 
  //MATRIX_ARB = 0x00000C09;‍‍‍‍‍‍‍‍‍‍‍

Have a nice day,

Jun Zhang

0 Kudos
Reply