capacitive touch of LPC845

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

capacitive touch of LPC845

1,301 次查看
1404387561
Contributor I

I use the capacitive touch of LPC845. When the finger touches the connected wire, the touch event occurs. If the finger is close to the wire, or if the finger is blocked by an insulating object and touched again, it can not trigger the touch event. What's the matter?

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,178 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

Please keep in mind that in this case the cover needs to be thin enough, and the metallic sensor needs to have a sufficient area for sensing.

Hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,178 次查看
1404387561
Contributor I

Thank you very much for your reply. I would like to ask you again if the contact surface is large enough and the lid is thin. Is it related to the capacitance connected to YH YL pins or what is the configuration of registers?

0 项奖励
回复

1,178 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

 

The sensitivity will depend on your PCB sensor pad design. I recommend you to read the document below, there are some guidelines to increase sensitivity in chapter 2.3 and some tests were made with different kinds of interference affecting the sensor in chapter 5.

 

https://www.nxp.com/docs/en/application-note/AN12083.pdf

 

Hope it helps!

 

Best regards,

Felipe

0 项奖励
回复