can communication error while receiving the data bytes in lpc4357 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can communication error while receiving the data bytes in lpc4357 board

808 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Fri Aug 29 20:51:49 MST 2014
hello,
        i am  using lpc4357 board provided by nxp (philips)....on the other hand i have an lpc17xx board,from  last few days i have been working for data transfer between these two boards via a CAN BUS.....i am using C_CAN0 peripheral in lpc4357 board ....it is working fine for the transmitting the databytes from lpc43xx to lpc17xx board....somehow i am not receiving the data or  any kind of interrupt on receiving end....i have tested lpc17xx board with other nodes it is working perfect ......i guess it is problem with the lpc43xx board while reception of the databytes...anybody please help me to crack this problem.....and suggest me a sample code for the C_CAN0 peripheral Tx and Rx....
             thanks....
标签 (1)
0 项奖励
回复
0 回复数