bypassing caps for power

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bypassing caps for power

883件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jbertalotto on Mon Dec 28 23:14:02 MST 2015
Hi,

I have been trying to find the documentation for powering the LPC1837, I am more concerned with the bypassing of the power. Is there any reference documentation on this topic for the LPC1837.

Thank you,
ラベル(1)
0 件の賞賛
返信
1 返信

868件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Wed Jan 13 07:44:00 MST 2016
No sure what you mean with "bypassing of the power". Maybe you want to have some more information about bypass capacitors.
This depends a little bit on your needs and also on the effort you can spend on a board.
The better the power supply structure is (supply itself and the PCB design), the less important the bypass capacitors are.
If you run the chip with high speed interfaces like the memory interface, then you should place, depending on your PCB design, suitable capacitors on the power supply pins to filter out the high frequency noise.
However, there is no fixed recommendation for this, it's more a rule of thumb thing. The only thing I could say is, that the standard 100nF caps used on most of the eval boards are not really the best choice for this. These values were more useful in the time of the 8MHz controllers.

Regards,
NXP Support Team.
0 件の賞賛
返信