boot from USB0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot from USB0

1,253 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by toad on Thu May 08 09:15:24 MST 2014
The Errata sheet for LPC4350/30/20/10 describes a potential race condition that effects endpoint 0. Is this bug present in the USB0 boot DFU ROM firmware (which communicates via endpoint 0) ? If so what is the suggested workaround to avoid this happening. Thanks.
Labels (1)
0 Kudos
Reply
1 Reply

1,245 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri May 09 11:58:30 MST 2014
Hi toad,

Yes , this is a bug and there is no work around for this as it happens during booting.

Thanks,
NXP Technical Support
0 Kudos
Reply