bit bang on LPC11Axx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bit bang on LPC11Axx

876 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gad on Thu May 14 04:46:17 MST 2015
Hi
I am trying to implement the bit bang on  I2c for LPC11Axx but have encounter a problem with the GPIO line,clock are not sync' etc'
I have build it based on an example from Keil (other chip)it seems that I have defines GPIO reg's SCL wrong.
Does any one have an bit banging  example on LPC11Axx ?
or correct define the macros : IODIR0,IOPIN0,PINSEL0,PINSEL1,IOCLR0,CCLK

Thanks and regards,
Yariv
Labels (1)
0 Kudos
Reply
0 Replies