best USBD mode for transceiving low rate data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

best USBD mode for transceiving low rate data

1,059件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dizgah on Sat Apr 02 21:05:29 MST 2016
Hi every one,I'm trying to use lpc11u68 for transceiving data between PC as host & MCU as a slave,data rate is about some KBPS,plug & play ability(without drivers limitations) is desired but not necessary,Simple initialing is desired too.
with this specifications which mode (CDC,HID,...) is desired?
EDIT: there is another usbd_rom_libusb mode in the LPCOPEN,seems is simpler to use for data transferring,in this state MCU recognized by PC in which mode(HID,CDC,...)?is this recommended for data transferring? and support plug & play or not ?
with best regards.
ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,003件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信