adding 3rd USB device controller port to LPC54608

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adding 3rd USB device controller port to LPC54608

ソリューションへジャンプ
2,322件の閲覧回数
belmontbob59
Contributor IV

I would like to add a 3rd USB device controller port to my MCU. I looked for parts and ended up with two solutions:

a) use FT120 which interfaces to MCU via parallel bus (http://www.ftdichip.com/Support/Documents/DataSheets/ICs/DS_FT120.pdf)

b)Use MAX4320E. This is SPI to USB  (https://www.maximintegrated.com/en/products/interface/controllers-expanders/MAX3420E.html)

is option(a) doable ? This means configuring the EMC to interface with FT120. I am worried about not getting EMC configured right. Option (b) looks simpler but I am worried about achieving lower USB bandwidth than If I was going with option (a) 

ラベル(2)
0 件の賞賛
返信
1 解決策
2,185件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Bob,

At the end, it is going to be your solution,  I do not see any problem to implement your Option A),  since EMC interface it is fast enough to get the data from a USB port, 

Hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,185件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Bob,

At the end, it is going to be your solution,  I do not see any problem to implement your Option A),  since EMC interface it is fast enough to get the data from a USB port, 

Hope this helps.

0 件の賞賛
返信
2,185件の閲覧回数
belmontbob59
Contributor IV

After doing some research on option A (FT120), I am confused on how to interface with the EMC.

FT120 has RD_n (Read Enable pin , active low) and WR_n (Write Enable pin, active low). However the EMC only provides us with EMC_WE .  WR_n will connect to EMC_WE but Where do I connect RD_n to ?

0 件の賞賛
返信