ablout Master Security Wrapper(MSW)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ablout Master Security Wrapper(MSW)

1,637 Views
superliyou
Contributor I

Hi ,

  Is there any more information about Master Security Wrapper(MSW)?  In UM11126 I only find below.

  where is it? How to set it and modify it? 

  47.3.3.3 Master Security Wrapper (MSW)
TrustZone for ARMv8-M offers IDAU functionality for CM33 when TrustZone feature is
configured. However, IDAU is not available for all other masters on LPC55S6x. A special
wrapper Master Security Wrapper (MSW) is implemented for each AHB Master except
CPU0.
MSW allows application to set security attribute for each master. There are two categories
of the MSW:
1. Simple Master: Bus Masters that can perform data access only: SDIO, USB-FS,
DMA0, DMA1, Hash-AES.
MSW for simple master enables strict checking by default. Secure data accesses can
access secure memory only. A programmable option to disable strict checking allows data
access from secure master to Non-secure memory.

  thanks a lot !

    

Labels (1)
0 Kudos
Reply
1 Reply

1,625 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

You can check all master security level (MSW) settings in the 47.4.73 Master secure level register section of the UM. Additionally, you can check the TrustZone examples included in our MCUXpresso SDK.

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 Kudos
Reply