ZigBee with NXP MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZigBee with NXP MCU

2,621 Views
lucasfontan
Contributor I

Hi, I would like to implement ZigBee protocol for my final thesis using a JN5168-001-M03Z module with an LPC1769, could it be possible? Has anyone done something similar? I need to use the LPC1769 because the JN5168-001-M03Z doesn´t has enough Pin Ports for my aplication. Thank you!

Labels (3)
0 Kudos
Reply
3 Replies

2,383 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Lucas,
You can implement the ZigBee protocol with the JN516800-001-M03Z also create an interface between the JN and the LPC.(SPI,UART..)
You can take a look for the next JN-AN-1189.

ZigBee Home Automation|NXP 

And you have to create a communication interface, the next user guide provide APIs for develop your own application
http://www.nxp.com/documents/user_manual/JN-UG-3087.pdf

Also, the LCP provides example for the development platform.
http://www.nxp.com/products/software-and-tools/hardware-development-tools/lpcxpresso-boards/lpcopen-...

Hope it helps
Mario

0 Kudos
Reply

2,383 Views
lucasfontan
Contributor I

Hi mario, thank you very much for your assistance.Nowadays I am not using JN516800-001-M03Z module because when I went to buy it, the seller had not stock, so I had to buy some XBee modules. Here in Argentina it is very difficult to get specific devices like JN516800-001-M03Z. I would like to have it but I couldn´t.

Regards,

Lucas.

0 Kudos
Reply

2,383 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Lucas,

I am sorry that you couldn't find stock. I wish you the best of luck on your project.

 

Regards,

Mario

0 Kudos
Reply