XIP and NON-XIP data transfer clarfication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XIP and NON-XIP data transfer clarfication

ソリューションへジャンプ
2,649件の閲覧回数
VIGNESH_BABU
Contributor II

Hi;

I was currently worked in LPC54018 customized Board.My Project is to display the font in the TFT Display (ST7789V).In our controller default  don't have an  internal flash Memory.So we install the External NOR Flash Memory(W25Q128JV) to interface with the Micro-controller and it is connected through TFT Display.

Doubts?

1.I have a doubt how the data was transfer whether through(External NOR flash -> SRAM -> TFT Controller[XIP METHOD]) or (External NOR Flash -> TFT Controller with the help of DMA[NON-XIP]).

2.How I was identified the path of data transfer in MCUXPresso Whether it was XIP or NON-XIP method?

0 件の賞賛
返信
1 解決策
2,630件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @VIGNESH_BABU 

 

XIP is execute directly in flash, no-xip is copy from flash to SRAM to execute.

About change NO-xip to XIP, if you use MCUXpresso IDE, try to disable "Plain load image" , the re-build.

Alice_Yang_0-1671171857379.png

 

 

Also there is XIP and NO-xip demo under SDK for lpc54s018, you can run them to check the process.

 

BR

Alice

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,631件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @VIGNESH_BABU 

 

XIP is execute directly in flash, no-xip is copy from flash to SRAM to execute.

About change NO-xip to XIP, if you use MCUXpresso IDE, try to disable "Plain load image" , the re-build.

Alice_Yang_0-1671171857379.png

 

 

Also there is XIP and NO-xip demo under SDK for lpc54s018, you can run them to check the process.

 

BR

Alice

 

 

0 件の賞賛
返信
2,599件の閲覧回数
VIGNESH_BABU
Contributor II

Hi Alice,

Finally I got the clarification of differences between XIP and NO-XIP. Thank you Alice.

0 件の賞賛
返信