Writing data to OM2NTP5332

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Writing data to OM2NTP5332

1,045件の閲覧回数
srgzsdf32
Contributor I

I am using the OM2NTP5332 NFC card with an Elatec TWN4 MultiTech 2 HF NFC reader/writer. I am trying to write some arbitrary data to the card (a type 5, ISO15693 64 bit card)

With a program called Director V4.50.1 I got with the reader from Elatec, I can read the ID and Tag Type from the NFC card as well as individual blocks of data from the card. However, I am unable to write any data to the card and I am unsure why.

It does work to write and read to the card using the NFC chip on my phone, which uses the ISO14443/MIFARE (32 bit) standard. Can you please advise me on what the problem might be and how I can resolve it? Could there some sort of security feature on the card that blocks the reader from writing to it but not my phone?

0 件の賞賛
返信
1 返信

1,034件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @srgzsdf32 

NTAG 5 can be read and written through the NFC of the mobile phone, so your problem should be in the reader, so it is recommended that you check whether the reader supports this type of tag write operation.

Best Regards,

kelly

 

0 件の賞賛
返信