Write-protect Flash sector in LPC1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Write-protect Flash sector in LPC1769

ソリューションへジャンプ
2,512件の閲覧回数
stenlarsson
Contributor II

Is it possible to write-protect sensitive Flash sectors in n LPC1769. I would like to store hw-part number etc. in a protected sector so that the information cannot be erased or overwritten by mistake or on purpose.

Is this possible?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,253件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sten Larsson,

   Unfortunately, the LPC1769 hardware still can't support the flash protection function now.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,254件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sten Larsson,

   Unfortunately, the LPC1769 hardware still can't support the flash protection function now.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,253件の閲覧回数
stenlarsson
Contributor II

Thank you!

0 件の賞賛
返信