Windows USB virtual com port drivers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows USB virtual com port drivers

2,753件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kbowers on Fri Sep 12 10:32:32 MST 2014
I am trying to use the Target USB connection with the USB ROM examples from LPCOpen.  I have a Windows 8.1 laptop and have downloaded the latest INF files for the USB drivers.

My problem is that when I plug in my LPC1549Xpresso V2 board, Windows doesn't recognize it at all so it doesn't install any drivers.

I also don't get a com port when I plug in the LINK DFU which I thought I should.  I had been using an LPCXpresso V2 board before with the MBED firmware and it always enumerated a com port when plugged in on the link connector.

Does anyone have any ideas on what I can try?
ラベル(1)
0 件の賞賛
返信
1 返信

2,262件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kbowers on Fri Sep 12 10:39:47 MST 2014
Additionally, since there is no comm port associated with the link interface, is there anywhere in LPCXpresso where I can view the "DEBUGOUT" messages that are in the LPCOpen examples?
0 件の賞賛
返信