Will newer version of spifi library be availible?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will newer version of spifi library be availible?

ソリューションへジャンプ
1,087件の閲覧回数
zhengyangqu
Contributor II

LPC SPIFI Peripheral|NXP 

SPIFI Library provided here seems to be outdated (Released: 12/11/2014).

I found lpcscrypt 2.0 software used an updated version of SPIFI lib, LPCScrypt v2.0.0|NXP 

will this library be available to be downloaded soon?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
967件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, as detailed on the LPCScrypt product page, LPCScrypt v2.0.0 no longer makes the use of LPC SPIFI library. Thus there is no associated update of the LPC SPIFI library.

The latest updates to the LPC SPIFI Library code base that I am aware of is that provided in the "LPC18_43_lpcspifilib_driver.zip" projects provided in the \Examples\Flashdrivers\NXP\LPC18_43 subdirectory of MCUXpresso IDE v10.2.1

Regards,

MCUXpresso IDE Support

元の投稿で解決策を見る

1 返信
968件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, as detailed on the LPCScrypt product page, LPCScrypt v2.0.0 no longer makes the use of LPC SPIFI library. Thus there is no associated update of the LPC SPIFI library.

The latest updates to the LPC SPIFI Library code base that I am aware of is that provided in the "LPC18_43_lpcspifilib_driver.zip" projects provided in the \Examples\Flashdrivers\NXP\LPC18_43 subdirectory of MCUXpresso IDE v10.2.1

Regards,

MCUXpresso IDE Support