Will an LPC11C24 run in "CAN Test" mode permanently?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will an LPC11C24 run in "CAN Test" mode permanently?

787 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LyraElectronics on Wed Feb 04 09:46:56 MST 2015
I would like to programattically set the CAN module to be silent on the bus (no ACK, no transmit).

If I set the TEST bit in the CANCTRL register, and then set the SILENT bit in then CANTEST register, will the CAN module receive messages as normal thereafter?

If so, are there any disadvantages to leaving the TEST bit set during running?

Thanks,
Mike
Labels (1)
0 Kudos
Reply
2 Replies

755 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Feb 04 11:42:19 MST 2015

Quote: LyraElectronics
Well, now I've tried it I can say that it certainly seems to work fine.

The CAN operation is exactly as normal, but with no transmission.

Does anyone know of any disadvantages of leaving the CAN module in TEST mode?



Silent mode is Silent mode  :D

If you just want to receive data, that's no problem...

At least if someone ACKs transmitted data (or are you working with DAR?)...

BTW: Which Baudrate are we talking about ?
0 Kudos
Reply

755 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LyraElectronics on Wed Feb 04 11:01:29 MST 2015
Well, now I've tried it I can say that it certainly seems to work fine.

The CAN operation is exactly as normal, but with no transmission.

Does anyone know of any disadvantages of leaving the CAN module in TEST mode?
0 Kudos
Reply