Why USB0 works, but USB1 does not work on HID LPCOPen project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why USB0 works, but USB1 does not work on HID LPCOPen project?

2,829件の閲覧回数
sharminsultanas
Contributor II

Hello

I am using code (NXPLPC1837/ NGXLPC1830xplorer)  from below site

LPCOpen Software for LPC18XX|NXP 

for NGX LPC1837 xplorer board.

However , in HID class keyboard project, only USB0 is enumerated as HID class device (keyboard). But  I wanted to use both USB0 and USB1 as HID class device.

In app_usbd_cfg.h it is written USB1 can be used instead of USB0 , by commenting  #define USE_USB0 and uncommentiing #define USE_USB1. However, it didnot work.

Can you please help me on solving this problem?

Regards

Sharmin

ラベル(3)
タグ(4)
0 件の賞賛
返信
1 返信

2,623件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Sharmin Sultana sheuly,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
I haven't replicated the same phenomenon according to your suggestion.
pastedImage_1.jpg
pastedImage_3.png
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信