Why RhPortStatus1 and RhPortStatus2 in USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why RhPortStatus1 and RhPortStatus2 in USB

2,039件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jayudhandha on Thu Jan 22 22:25:31 MST 2015
Hello,

I am not able to understand the reason of RhPortStatus1 and RhPortStatus2 this two ports are used in usb interfacing. Why two?

Regards,
Jayesh dhandha
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,030件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jayudhandha on Sat Jan 24 02:47:21 MST 2015
Not able to understand the difference between HcDoneHead and
HccaDoneHead.
0 件の賞賛
返信

2,030件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jayudhandha on Sat Jan 24 00:45:49 MST 2015
Yes i got your mail. And i got the answer as well. :-)

0 件の賞賛
返信

2,031件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Jan 23 04:07:03 MST 2015
Because the built in host controller hardware can have up to two ports.
Whether or not each possible port actually is a host port is controlled
by the setting of the PORTSEL register (Table 315 in latest UM10470)

Presumably, if a particular port is not set as host, no status change or interrupt
bits for that port will be set.

Mike.
0 件の賞賛
返信

2,029件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Jan 23 03:52:18 MST 2015
Why have your other USB Host posts disappeared -- taking my replies with them.
Did you get the document in my email?

Mike
0 件の賞賛
返信