Why LPC1768 do not run ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why LPC1768 do not run ?

1,765件の閲覧回数
alexshest
Contributor I

Hello!

I have a problem.

I have two devices, as shown in the figure.

LPC1768.PNG

I do the following:

1. I connect the power of device 2 through the connector xp2

2. I connect line1 of device 2 to devise 1 through the connector xp3

3. I connect the power connector and ground connector to xp1

4. and lpc1768 do not run!!!

What is this magic? Why lpc1768 do not run? What I missing?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,613件の閲覧回数
alexshest
Contributor I

P2.10 at high , controllet not at a boot state.

Its a valid user program .

If we сhange the sequence to:

1. I connect the power of device 2 through the connector xp2

2. I connect the power connector and ground connector to xp1

3. I connect line1 of device 2 to devise 1 through the connector xp3

4. and lpc1768 work fine

0 件の賞賛
返信

1,613件の閲覧回数
sergedemaseneer
Contributor III

Is P2.10 high at boot? (otherwise the chip is in programming mode) and is there a valid user program with correct checksum in the controller?

0 件の賞賛
返信