Which root filesystem for ucLinux on 1788? How to install?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which root filesystem for ucLinux on 1788? How to install?

1,190 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lkoziarz on Thu Sep 26 14:38:28 MST 2013
Hi there,

I'm working on a custom LPC1788 design that has 8MB SDRAM and 8MB NOR Flash.  I'm trying to get uBoot and ucLinux running on this system.

So far I've modified uBoot to get SDRAM and Flash working and it runs no problem.  I've built the kernel for the 1788 from ucLinux's sources and emcraft's patches and it seems to compile and copy over correctly.  But the kernel hard faults right after handover, I'm guessing because it has no filesystem to attach to.

Does anyone have some howtos on building a filesystem (initramfs? romfs?) for the ucLinux build and creating the final uImage?

And where do you guys prefer it goes?  Are you copying to RAM and booting from there?  XIP from Flash? (That script seems to be broken at the moment).

I know I'm close and I know others have done this, but there's not much information out there. 

Thanks!
Labels (1)
0 Kudos
Reply
1 Reply

1,178 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jupiter on Fri Sep 27 07:35:32 MST 2013
I'am trying the same thing but I've not managed to compile yet. I'am new to the linux world.
I'am using this board :
open1788

Can't help yet.

Regards.
0 Kudos
Reply