Which IDE, LPCXpresso or MCUXpresso ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which IDE, LPCXpresso or MCUXpresso ?

Jump to solution
2,203 Views
anaseem
Contributor IV

User Manual says LPC11E68JBD48E is ARM Cortex-M0+ based.

Following is note from NXP Website:

NOTE: MCUXpresso IDE is now recommended for developers using LPC Cortex-M based microcontrollers.

Please confirm that LPC11E68JBD48E is not Cortex-M based ?

Labels (1)
1 Solution
2,035 Views
converse
Senior Contributor V

Use MCUXpresso. LPC11xxx is a Cortex-M device.

View solution in original post

2 Replies
2,035 Views
soledad
NXP Employee
NXP Employee

Hi,

I suggest to use MCUXpresso.

MCUXpresso IDE contains built in support for a slightly extended set of LPC Cortex-M based parts that were supported in LPCXpresso IDE v8.2.2.
LPC Cortex-M include Cortex-M0+ devices.

MCUXpresso IDE supports the LPC11E68JBD48


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,036 Views
converse
Senior Contributor V

Use MCUXpresso. LPC11xxx is a Cortex-M device.