Where's the loc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where's the loc

995 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Sat Jan 03 01:58:40 MST 2015
On an LPC11xx there are several registers called IOCON_SCK_LOC, IOCON_DSR_LOC etc. which select pin locations.

The LPC11E67 also has movable functions but I see no similar registers. Have I just failed to find them? Are they called something different? or does the 11E67 manage without them.  If so, what happens if the same function gets mapped to two different pins in the IOCON registers? (OK you can tell me "Don't do that, it's stupid")
Labels (1)
0 Kudos
Reply
0 Replies