Where's the loc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where's the loc

988件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Sat Jan 03 01:58:40 MST 2015
On an LPC11xx there are several registers called IOCON_SCK_LOC, IOCON_DSR_LOC etc. which select pin locations.

The LPC11E67 also has movable functions but I see no similar registers. Have I just failed to find them? Are they called something different? or does the 11E67 manage without them.  If so, what happens if the same function gets mapped to two different pins in the IOCON registers? (OK you can tell me "Don't do that, it's stupid")
ラベル(1)
0 件の賞賛
返信
0 返答(返信)