Where have the IOH libraries gone for the LPC11U37H?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where have the IOH libraries gone for the LPC11U37H?

1,853件の閲覧回数
shareefjalloq
Contributor II

Hi,

I've got some very old IOH libraries for the 11U37 and was just looking to see if they'd been updated since 2013 but they seem to have disappeared.  Any idea where the libraries and documentation have gone?  Even searching for an app note such as AN11471 doesn't turn up anything.

Thanks.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,703件の閲覧回数
shareefjalloq
Contributor II

Perhaps this block has died a death and the current recommended path is to use the SCT to generate similar waveforms?  I'm wanting to handle Dali tx/rx using Manchester Encoding and I found an SCT example for RC5 IR tx/rx.  Am I better off going down that route?

0 件の賞賛
返信

1,703件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Shareef Jalloq,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Any idea where the libraries and documentation have gone?
-- You can find the libraries and documentation via the below link.
https://community.nxp.com/docs/DOC-330808
2) Am I better off going down that route?
-- Yes, I agree with you。
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信