Where can I download the Windows 7 USB drivers for LPC1549?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where can I download the Windows 7 USB drivers for LPC1549?

2,122 次查看
isaotakashima
Contributor IV

I would like to check if below project works property.

lpcopen_2_20_keil_iar_nxp_lpcxpresso_1549\applications\lpc15xx\examples\usbd_rom\cdc_vcom

I already check above project woks property on Windows 10 PC.

Then I want to check if above project works property on Windows 7 PC.

Then I try to download the Windows 7 USB drivers for LPC1549 at below links.

https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcop...

https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fnxpfile%2F...

Unfortunately, I cannot download it from above links.

Please tell us where can I download the Windows 7 USB drivers for LPC1549.

Best regards,

Takashima

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

2,005 次查看
FelipeGarcia
NXP Employee
NXP Employee


This issue was solved by removing INTERFACE_ASSOCIATION from bDeviceProtocol in device descriptor.

-------------------------------------------------------------------------------
Note:

This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore.
-------------------------------------------------------------------------------

0 项奖励
回复