When will IBIS models be available for the LPC4357FET256 or can any alternatives be used

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When will IBIS models be available for the LPC4357FET256 or can any alternatives be used

839 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pricey on Mon Feb 20 03:18:34 MST 2012
Hi - I will be starting PCB layout soon for the LPC4357FET256 and will need IBIS models for simulation
1. When will they be available?
2. Presumably they will be the same as those for the LPC4350 in which case when will they be available?
3. I believe that the LPC4350 is very similar to the LPC1850 (apart from M3 vs M4/M0!) would those IBIS models be useable and if so when will they be available?
4. Would the IBIS models for the LPC178x be at all useable / adaptable for this (note looks like different packages)?
Cheers,
Pricey
Labels (1)
0 Kudos
Reply
0 Replies