What's the lowest ADC reference voltage I can use for the LPC1114 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What's the lowest ADC reference voltage I can use for the LPC1114 ?

1,069 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by UncleJoe on Sun Jun 22 15:01:15 MST 2014
I'm wondering if I can directly measure the heart's  ECG with a micro controller.

I need very high accuracy (in the sub mV range), but very low bandwidth. I've tried putting together a circuit with the ADC voltage reference (VDDA) set to 0.1V, but no matter what, my ADC readings are always 1023.

I don't see the minimum reference voltage mentioned in the documentation. Is there one?
标签 (1)
0 项奖励
回复
2 回复数

984 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Thu Jul 03 15:40:15 MST 2014
Hi,

On the LPC1114, the VDD supply is internally tied to the ADC internal reference voltage and analog supply.
Thanks.

nxp_support
0 项奖励
回复

984 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Sun Jun 22 16:00:51 MST 2014
VDDA is not Voltage Reference  :exmark:

Use a microcontroller with Voltage reference Input   :)

Something like LPC15xx with VREFP_ADC pin (and fast 12bit Converter) ...
0 项奖励
回复