What's the difference between the NHS3100 and LPC8N04

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What's the difference between the NHS3100 and LPC8N04

3,537 次查看
raven_coda
Contributor I

I've compared these two offerings' datasheets, which look almost identical. Can someone point out what the difference is?

 

Thanks

0 项奖励
回复
2 回复数

3,527 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have to admit the two silicons are almost  the same from perspective of core, pin assignment, functions, features.

But the MHS3100 has multiple packages, the LPC8N04 just has one package.

Pls refer to section 7 Pinning.

I attach the data sheet of both silicons.

BR

XiangJun Rong

 

0 项奖励
回复

3,525 次查看
raven_coda
Contributor I

Thanks for the quick reply. I did notice the different footprint options for the NHS3100. If that's the only difference then I'll just assume the NHS3100 supersedes the LPC8N04.

0 项奖励
回复