What's the difference between the NHS3100 and LPC8N04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the difference between the NHS3100 and LPC8N04

3,521件の閲覧回数
raven_coda
Contributor I

I've compared these two offerings' datasheets, which look almost identical. Can someone point out what the difference is?

 

Thanks

0 件の賞賛
返信
2 返答(返信)

3,511件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have to admit the two silicons are almost  the same from perspective of core, pin assignment, functions, features.

But the MHS3100 has multiple packages, the LPC8N04 just has one package.

Pls refer to section 7 Pinning.

I attach the data sheet of both silicons.

BR

XiangJun Rong

 

0 件の賞賛
返信

3,509件の閲覧回数
raven_coda
Contributor I

Thanks for the quick reply. I did notice the different footprint options for the NHS3100. If that's the only difference then I'll just assume the NHS3100 supersedes the LPC8N04.

0 件の賞賛
返信