What is the state of IO during the period from power-on to boot on MCU LPC32?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the state of IO during the period from power-on to boot on MCU LPC32?

1,226 次查看
Guestsun
Contributor II

What is the state of IO during the period from power-on to boot on MCU LPC32?

0 项奖励
回复
2 回复数

1,213 次查看
frank_m
Senior Contributor III

In a tristate mode, effectively off.

A common feature of all ARM Cortex M devices is, all peripheral units must be explicitely enabled (clock and power) to operate.
These peripherals are by default off at reset.

Very few exceptions might apply, like dedicated quartz input pins or JTAG/SWD pins.

0 项奖励
回复

1,202 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to data sheet of LPC32xx, the attribute of a pin is input(I), Output(O), bidirectional(I/O) , analog, power.

For the bidirectional I/O pin and Input pin, I suppose that the state of IO during the period from power-on to boot are in input mode, except for JTAG pins.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1711606609838.png

 

0 项奖励
回复