There could be an error on rev E and rev F schematics of LPCXpresso546 (OM13098) board.
The onboard SDRAM is a 128Mb Winbond's W9812G6JB-6I which has no A12 pin. However the schematics show as if such non-existing pin was connected, which only applies to a 256Mb chip, e.g Winbond's W9825Gxx.
Is this so? And for complete clarity, how should the 128Mb SDRAM be connected with the highest LPC546's external memory controller address pins EMC_A14, EMC_A13, EMC_A12 on corresponding BA1, BA0 and A11 ?
Attached image of SDRAM pins.
Thanks
解決済! 解決策の投稿を見る。
Hi Pablo,
Thanks for your feedback. This is not an error, this pin is connected to support a 256Mb SDRAM expansion as you mention.
Other than that, 128Mb SDRAM should be connected as schematics show.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Pablo,
Thanks for your feedback. This is not an error, this pin is connected to support a 256Mb SDRAM expansion as you mention.
Other than that, 128Mb SDRAM should be connected as schematics show.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------