What is the recommended way to evaluate LPC4370 80MSPS without LabTool?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the recommended way to evaluate LPC4370 80MSPS without LabTool?

1,260 次查看
brandon1
Contributor I

LabTool (LabTool link) is now a Non-stock product from Embedded Artists requiring a MOQ of 250.  Is there another suggested method to evaluate the LPC4370 and its internal 80MSPS ADC?

Thanks,

Brandon

标签 (1)
0 项奖励
回复
1 回复

1,167 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

NXP doesn't have similar product of LABTOOL as replacement.

I would suggest you check with Embedded Artists distributors if you can order one piece.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复