What is the recommended way to evaluate LPC4370 80MSPS without LabTool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the recommended way to evaluate LPC4370 80MSPS without LabTool?

1,263 Views
brandon1
Contributor I

LabTool (LabTool link) is now a Non-stock product from Embedded Artists requiring a MOQ of 250.  Is there another suggested method to evaluate the LPC4370 and its internal 80MSPS ADC?

Thanks,

Brandon

Labels (1)
0 Kudos
Reply
1 Reply

1,170 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

NXP doesn't have similar product of LABTOOL as replacement.

I would suggest you check with Embedded Artists distributors if you can order one piece.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply