What is the recommended microcontroller series that replaces the LPC213x series?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the recommended microcontroller series that replaces the LPC213x series?

跳至解决方案
1,760 次查看
kk7xo
Contributor III

It's my understanding that the LPC213x series is not recommended for new designs.  What series recommended for new designs has roughly equivalent capability (Memory size, speed, peripherals, etc.)?

标签 (1)
0 项奖励
回复
1 解答
1,644 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Albert,

The LPC21xx is Not Recommended In New Design, I suggest you refer to the LPC5411x and check if it meets your requirement.

LPC541XX | NXP 

But the LPC541xx does not have EMC module, so it can not hook with external SRAM, flash.

You can also check LPC51U68 for low cost solution:

LPC51U68 | NXP 

Hope it can help you

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,645 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Albert,

The LPC21xx is Not Recommended In New Design, I suggest you refer to the LPC5411x and check if it meets your requirement.

LPC541XX | NXP 

But the LPC541xx does not have EMC module, so it can not hook with external SRAM, flash.

You can also check LPC51U68 for low cost solution:

LPC51U68 | NXP 

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复