What is IP3516HS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is IP3516HS?

跳至解决方案
3,333 次查看
victorpecanins
Contributor II

In the USB host example projects for LPCXpresso54608, there are three possible options for the USB peripheral: OHCI, EHCI and IP3516HS. OHCI is for USB FS, EHCI for HS, and IP3516HS apparently also for HS. This name does not appear on the datasheet, nor in the forums, not even a Google search gives any clue.

So, what is IP3516 and why is it used for?

Regards

标签 (2)
0 项奖励
回复
1 解答
2,925 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi  VIctor Pecanins ,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
The IP3516HS is a inter code of a USB HOST controller interface, the other macros can be used to enable to respective USB HOST controller interface.
You can learn the more detailed information about the USB HOST controller interface via the following link.
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,926 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi  VIctor Pecanins ,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
The IP3516HS is a inter code of a USB HOST controller interface, the other macros can be used to enable to respective USB HOST controller interface.
You can learn the more detailed information about the USB HOST controller interface via the following link.
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
0 项奖励
回复