What is Chicken Bit in validation ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is Chicken Bit in validation ?

14,196件の閲覧回数
saikrish417
Contributor II

is it in iP or cpu , can any one tell Please ?

ラベル(1)
タグ(2)
1 返信

13,775件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

The question comes with no relation to a specific product, so it's hard to interpret what you want to know.

"Chicken bit" is a general term used in silicon chip design, for example for our MCUs and MPUs.

It is a bit which can be used to enable/disable functional blocks inside the chip. This can be IP blocks like Ethernet MAC or CAN, but also additional CPU blocks. We use this method to offer various chip configurations to the market based on the same silicon die. Normally these bits are OTP (one-time-programmable) and they are not accessible by the end user. We program these bits during production on the chip tester and then this area is locked against further access.