Watchdog and ISP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog and ISP mode

918件の閲覧回数
abele_barbieri
Contributor I

Hello,
I'm using LPC51U68 for a customer board, and now I'tring to enter the ISP UART mode by calling from user code the IAP_ReinvokeISP() function.
The LPC answers to "Syncronized" starting messages, and enters in ISP UART mode.
Unfortunately, after the programmed time, the Watchdog resets the board and the application code restart (causing exit from ISP mode).
There is a way to solve/handle this issue?

Thanks 

Abele

0 件の賞賛
返信
1 返信

890件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello @abele_barbieri,
My suspect is that the watchdog is being triggered on the bootloader side. So I will suggest disabling the watchdog and any interruption before calling the ISP reinvoke. However as mentioned in the chapter 17.6.1 called Watchdog mode register "Once the WDEN, WDPROTECT, or WDRESET bits are set they cannot be cleared by software. Both flags are cleared by an external reset or a Watchdog timer reset."
Could you try doing a software reset for the peripheral? The following API should help:
RESET_PeripheralReset(kWWDT_RST_SHIFT_RSTn);

BR
Habib

0 件の賞賛
返信