Watchdog and ISP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog and ISP mode

909 Views
abele_barbieri
Contributor I

Hello,
I'm using LPC51U68 for a customer board, and now I'tring to enter the ISP UART mode by calling from user code the IAP_ReinvokeISP() function.
The LPC answers to "Syncronized" starting messages, and enters in ISP UART mode.
Unfortunately, after the programmed time, the Watchdog resets the board and the application code restart (causing exit from ISP mode).
There is a way to solve/handle this issue?

Thanks 

Abele

0 Kudos
Reply
1 Reply

881 Views
Habib_MS
NXP Employee
NXP Employee

Hello @abele_barbieri,
My suspect is that the watchdog is being triggered on the bootloader side. So I will suggest disabling the watchdog and any interruption before calling the ISP reinvoke. However as mentioned in the chapter 17.6.1 called Watchdog mode register "Once the WDEN, WDPROTECT, or WDRESET bits are set they cannot be cleared by software. Both flags are cleared by an external reset or a Watchdog timer reset."
Could you try doing a software reset for the peripheral? The following API should help:
RESET_PeripheralReset(kWWDT_RST_SHIFT_RSTn);

BR
Habib

0 Kudos
Reply