Wake-up LPC17xx using GPIO interrupt with 3V3 regulator supply only

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wake-up LPC17xx using GPIO interrupt with 3V3 regulator supply only

698件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by da on Mon Jun 02 08:44:24 MST 2014
I would like to use some pins of GPIO port 0 to wake-up my LPC17xx controller.
The manual tells me that, if I configure the correct GPIO Interrupt Enable registers,
a rising/falling edge of one of these GPIO pins could bring my controller out of sleep mode or power-down mode.

My hardware provides 2 separated power domains: one 3.3V supply for the I/O pads (VDD 3V3), and one 3.3V supply for the CPU (VDD REG 3V3).
When the application is in sleep mode or power-down mode, the 3.3V supply for the I/O pads is disconnected for power consumption reason,
and only the 3.3V supply for the CPU (the on-chip regulator) is available.

Do you think that my GPIO port 0 interrupt can still wake-up my controller if there is no 3V3 VDD supply for the I/O pads ?

Thx,

da
ラベル(1)
0 件の賞賛
返信
1 返信

647件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Wed Jun 04 17:02:29 MST 2014
Hi,

You have to keep the I/O Vdd supply on. If you configure the GPIOs appropriately and make sure there is no contention on the port pins, the I/O current should not influence the total current.

Thanks.

nxp_support
0 件の賞賛
返信