WE need a Controller which support CAN, LIN and USB2.0.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WE need a Controller which support CAN, LIN and USB2.0.

1,933件の閲覧回数
ipsitamishra
Contributor I

We found LPC2925FBD100, but we are not sure this is still in production or not, Could you please help on this? It has mentioned the controller is not recommended for new design? So if we will use we will get any support from NXP or not?

And Please help on us to find another low cost controller which support CAN , LIN and USB.

0 件の賞賛
返信
3 返答(返信)

1,827件の閲覧回数
ipsitamishra
Contributor I

Hi can you please let me know which best low cost  LPC Evaluation bored for the above features. (can, lin functionality) ? 

0 件の賞賛
返信

1,827件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer and select below boards for LPC MCU CAN/LIN function evaluation:

OM13094: LPCXpresso54618 CAN-FD kit

KIT33662LEFEVBE: Evaluation Kit - MC33662L, LIN2.1/SAEJ2602-2, LIN Phy

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,827件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

LPC2925FBD100 isn't a up to date product.

We would recommend customer to refer and use below platform products:

LPC540xx MCU Family, such as: LPC54016JBD100E, LPC54016JBD208E, LPC54018JBD208E

Kinetis K22_120MHz MCU family, such as: MK22FN1M0AVLH12, MK22FN1M0AVLQ12

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信